earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Enterprise Central, Enterprise Server, FDP Server, WorkStation
Functionalities: Trends
10/30/2025

Creating a Real-Time Plot Trend Chart

You create a real-time plot trend chart to display a variable in real time.

Show More
action_close

The real-time plot is a variable displayed directly in the trend chart. The real-time plot is an instant reflection of the variable, so the history of the real-time plot is lost when the trend chart is closed. However, the history is not lost for I/O points that have implicit logs where approximately 500 records of history are displayed.

 
action_zoom_plus_stroke Real-time plot, schematic
Figure: Real-time plot, schematic

A real-time plot trend chart updates and draws a solid series each time it registers that the variable has a new value. If the variable remains on the same value, the series is drawn as a dotted line.

When you save a real-time plot trend chart, a trend chart object is created that you can reach from the System Tree pane.

Note:
  • A real-time plot can only be displayed in a trend chart and not in a trend log list.

To create a real-time plot trend chart
  1. In WorkStation, in the System Tree pane, select the variable you want to display in a real-time plot trend chart.

  2. On the Actions menu, point to View and then click New Trend chart.

  3. Click the Save button

     
    action_zoom_plus_stroke
    .

  4. Browse to where you want to save the real-time plot trend chart.

  5. Click Save .

By saving the real-time plot trend chart, a trend chart object is created in the System Tree pane.

  • Real-Time Plotting
  • Trend Chart View
  • Saving the Trend Chart Settings