earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Enterprise Central, Enterprise Server, Esmi Sense FDP
Functionalities: Trends
12/3/2024

Creating a Variable Triggered Trend Log

You create a variable triggered trend log to record the variable according to the changes of an associated trigger variable.

Show More
action_close

​The variable triggered trend log records the variable when the conditions of the associated trigger variable are met. Use this type of trend log when the log interval is scheduled to log monthly or yearly, or when another device is used to trigger the log.

For example, in the figure below, the variable triggered trend log records a variable every time the associated trigger variable, for example, a switch, changes to true. The records are printed in a trend chart. Notice that the variable triggered trend log records the variable without any regard to time or delta.

 
action_zoom_plus_stroke Variable triggered trend log schematic
Figure: Variable triggered trend log schematic

You can configure the trend log to collect data when the trigger value changes to True, changes to False, or All changes.

 
action_zoom_plus_stroke Trigger variable changes to true
Figure: Trigger variable changes to true
 
action_zoom_plus_stroke Trigger variable changes to false
Figure: Trigger variable changes to false
 
action_zoom_plus_stroke Trigger variable all changes
Figure: Trigger variable all changes
Variable triggered trend log meter functionality

A variable triggered trend log can be created with initial meter settings. The variable triggered trend log supports the meter change command and meter consumption calculation. You can view the last meter change information on the variable triggered trend log object. For more information, see Meter Function .

To create a variable triggered trend log
  1. In WorkStation, in the System Tree pane, select the folder or EcoStruxure BMS server where you want to create the trend log.

  2. On the File menu, point to New , and then click Trend .

  3. In the Create Object wizard, in the object type list, select Variable Triggered Trend Log .

  4. In the Name box, type a name for the trend log.

  5. In the Description box, type a description.

  6. Click Next .

  7. In the Configure Variable Triggered Trend Log page, in the Logged variable box, enter the variable you want to log.

  8. Click the Set unit button

     
    action_zoom_plus_stroke
    .

  9. In the Unit selection dialog box, select a unit for the trend log values.

  10. In the Prefix box, select the prefix of the unit.

  11. Click Select .

  12. In the Trigger variable box, enter the variable that triggers the log.

  13. In the Trigger condition box, select Change to true to log the variable when the trigger variable changes to true.

  14. In the Log size box, select the number of records to be stored before old records are overwritten.

  15. In the Available trend storage box, check that the available number of records is not exceeded.

  16. In the Clear when enabled box, select True to clear the trend log every time the trend log is enabled.

  17. Click Next .

  18. In the Initial Meter Settings page, in the Set initial meter box, select True to enable the meter function.

  19. In the Start time box, enter the time when the meter was installed.

  20. In the Start value box, enter the value of the new meter when it was installed.

  21. In the Min value box, enter the first value of the new meter after roll-over.

  22. In the Max value box, enter the last value of the new meter before roll-over

  23. Click Next .

  24. In the Connect Objects to the Trend Log page, in the Extended Trend Log box, click the Browse button to create an extended trend log and connect it to the trend log.

  25. In the Trend Log List box, click the Browse button to create a trend log list and connect it to the trend log.

  26. In the Trend Chart box, click the Browse button to either create a new trend chart or connect the trend log to an existing trend chart.

  27. Click Create .

The variable triggered trend log is created in the selected folder.

  • Variable Triggered Trend Logs
  • Trend Units
  • Log Record Storage
  • Meter Function
  • Create Object Dialog – Naming the Object Page
  • Create Trend Log Wizard – Configure Change of Value Trend Log Page
  • Create Trend Log Wizard – Initial Meter Settings Page
  • Creating an Extended Trend Log
  • Creating a Trend Log List
  • Creating a Trend Chart that Monitors a Trend Log Series