Use the Configuration page to configure the port number the Enterprise Server listens to when communicating through a specific protocol.
|
Component |
Description |
|
HTTP Port |
Type the port number that the Enterprise Server listens to when communicating through the Hypertext Transfer Protocol. |
|
HTTPS Port |
Type the port number that the Enterprise Server Server listens to when communicating through a secure version of the Hypertext Transfer Protocol. |
|
TCP Port |
Type the port number that the Enterprise Server listens to when communicating through the Transmission Control Protocol. |