earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Basic Functionality
12/3/2024

Event Styles Dialog Box

Use the Event Styles dialog box to edit the fonts and colors for different events in the Events pane and Event View.

 
action_zoom_plus_stroke Event Style dialog box
Figure: Event Style dialog box

Table: Event Style Dialog Box

Component

Description

 
action_zoom_plus_stroke

Ad d style

Click to add and configure a new event to style.

 
action_zoom_plus_stroke

Delete style

Click to remove an event style.

 
action_zoom_plus_stroke

Move up

Click to increase the priority of an event.

 
action_zoom_plus_stroke

Move down

Click to decrease the priority of an event.

Priority

Enter the priority of the event to style.

Condition

Enter the condition or conditions of the event to style.

Background color

Enter the background color of the row for events in the Events pane and Event View that fulfill the configured conditions.

Font color

Enter the font color to use for events in the Events pane and Event View that fulfill configured conditions.

Font

Enter the font to use for events in the Events pane and Event View that fulfill configured conditions.

  • Events Pane and Event View Customization