earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, Esmi Sense FDP
Functionalities: Basic Functionality
12/3/2024

Event View Properties

Use the Event View properties for viewing and editing the properties of the Events pane and Event View.

 
action_zoom_plus_stroke Event View properties
Figure: Event View properties

Table: Event View Properties

Component

Description

Show milliseconds

Select True to display time properties including milliseconds.

Number of records shown

Enter the number of rows you want to list in the Events pane or Event view. You can enter any number between 1 and 5999.

Important:
  • By default, the latest 1000 event records are displayed in the Event View.

  • Regardless of the number of event records in the database, you can display a maximum of 5999 event records at a time in the Event View.

  • You can use the filter to display a different set of event records, maximum 5999 records at a time.

  • Events Pane and Event View Customization