earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Trends
10/30/2025

Extended Trend Log Properties – Basic Tab

Use the Basic tab to configure the Extended trend log.

 
action_zoom_plus_stroke Extended Trend Log properties - Basic Tab
Figure: Extended Trend Log properties - Basic Tab

Table: Extended Trend Log Properties - Basic Tab

Component

Description

Monitored trend log

Enter the path to the trend log you want to transfer records from.

Unit

The unit of an extended trend log created from the trend log wizard at the same time as the connected trend log inherits the unit of measurement from the connected trend log.

The unit of an extended trend log that is manually connected to a trend log needs to be manually configured to use the same unit of measurement as the connected trend log.

Smart log

Select True to optimize the transfer of the monitored trend log to the extended trend log.

Threshold

Select the percentage threshold at which the trend log transfers its records to the extended trend log.

Maximum transfer interval

Select the maximum length of time that can pass between transfers from the monitored trend log to the extended trend log.

Transfer trigger variable

Enter a trigger variable to force a transfer of all records from the trend log to the extended trend log, for example, to generate a complete report.

For more information, see Extended Trend Logs .

Log size

Select the number of records to store before old records are overwritten, including internal records generated by the trend log.

For more information, see Log Record Storage .

Include in report s

Select True to include the extended trend log data in reports.

  • Extended Trend Logs
  • Configure Dialog Box – Operation Tab
  • Configure Dialog Box – Configuration Tab
  • General Information Properties – Basic Tab
  • References Tab
  • Records Are Not Transferred to the Extended Trend Log