earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WorkStation
Functionalities: Basic Functionality
12/2/2024

Forcing a Value

You force a value when you want to override a value, such as a value from a device.

Show More
action_close

When you force a value, you override all input from the system. For example, if a schedule is set to enable a device at 09:00, but you want to enable it at 08:00, you can force the enablement at 08:00.

You can manually release a forced value at any time or you can automate the release, using a Timed Force utility object to specify the duration or end time of the force. For more information, see Timed Force Objects .

When you release a forced value, the value returns to its normal status.

In WorkStation, you can view the unforced value, which is the real value from the system, at any time. For more information, see Viewing an Unforced Value .

Timeout on forced values

You can set a timeout on forced values so that the forced value is automatically unforced after a fixed time. The time can be a duration, for example two hours. The forced value can also be unforced at a specific calendar date and time.

For more information, see Setting a Timeout on a Forced Value .

For more information, see Setting a Timeout on a Forced Value WebStation .

Indication in WorkStation

A forced value is indicated by orange color in the properties dialog boxes. In in the Watch pane, a forced value is indicated by a pointing hand

 
action_zoom_plus_stroke
.

In the List View and Search View, a forced value is indicated by the text [Forced] in the 'Value' column.

In WorkStation, you can view the unforced value, which is the real value from the system, at any time. For more information, see Viewing an Unforced Value .

Indication in WebStation

A forced value is indicated by orange color and a pointing hand in the List view.

Indication in Function Block Graphics Viewer

A forced value is indicated by orange color in Function Block Graphics Viewer. For more information, see Forced Value Indication in Function Block Graphics Viewer .

Search for forced values

You can search for forced values using the search function in WorkStation.

For more information, see Searching for Forced Values .

You can search for forced values in WebStation using Diagnostics.

For more information, see Displaying a List of Forced Values in WebStation .

To force a value
  1. In WorkStation, in the System Tree pane, select the value you want to force.

  2. On the File menu, click Properties .

  3. Change the value.

  4. Click Force .

  5. Click OK .

  • Forced Values
  • Changing Value Dialog Box
  • Force and Unforce Buttons
  • Releasing a Forced Value
  • Viewing an Unforced Value
  • Searching for Forced Values
  • Setting a Timeout on a Forced Value