earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WorkStation
Functionalities: Basic Functionality
12/2/2024

Hiding Menus and Toolbars

You hide the main menus and toolbars if you do not use them or think they take up to much space.

Show More
action_close

​You can increase the Work area in WorkStation by using Full screen mode and hiding toolbars and panes.

Hide Toolbars and Panes

You can increase the work area in WorkStation by hiding some or all of the toolbars and panes. Most functions can still be reached using the right-click method. All toolbars and panes that are hidden can be displayed again at any time.

In this example, the System Tree pane, Address bar, Basic toolbar, and Main menu are hidden.

 
action_zoom_plus_stroke Default workspace (top left) and a workspace with the System Tree pane, Address bar, Basic toolbar, and Main menu hidden (bottom right).
Figure: Default workspace (top left) and a workspace with the System Tree pane, Address bar, Basic toolbar, and Main menu hidden (bottom right).

Full Screen Mode

To further increase the Work area you can use Full screen mode. This function maximizes the window in focus to fill the whole screen. This is a good function to use, for example, when you work in large graphics with lots of information.

 
action_zoom_plus_stroke Full screen mode
Figure: Full screen mode

To hide menus and toolbars
  • In WorkStation , click View , point to Toolbars , and then click the menus and toolbars you want to hide.

  • Increase the Work Area in WorkStation
  • Menu Bar
  • Hiding Panes