earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: WorkStation, WebStation
Functionalities: Alarms
12/3/2024

Alarm Attachments

You can add attachments to alarm objects, except System Information alarms. An attachment is a link pointing to an object in the system. When an alarm that has an attachment is triggered, a paperclip icon is displayed in the Alarms pane and Alarm Views. It is also possible to configure the attachment to display when the alarm is going from Normal to Alarm state.

An attachment can be: a voice message, a report, a trend chart, a schedule, a Microsoft Word file, a PDF file, a video recording, or a pop-up window that contains information regarding the alarm.

You can add the same attachment or set of attachments to multiple alarms in a single operation. You can also delete the attachments that belong to multiple alarms in a single operation. If you add an attachment that already has been attached to an alarm, the later attachment is added as a duplicate.

You can open attachments provided that the program or editor associated with the attachment is locally installed on your computer. For example, if the attachment is a PDF file, you can open the file if Adobe Reader or a similar program is installed on your computer.

  • How Alarms Work
  • Alarm Functions
  • Alarms Pane and Alarm View
  • Alarms Pane and Alarm View Icons
  • Alarms Pane Context Menu
  • Opening an Alarm Attachment
  • Opening an Alarm Attachment in WebStation
  • Adding an Attachment to an Alarm
  • Adding an Attachment to an Alarm using WebStation
  • Removing an Attachment from an Alarm
  • Removing an Attachment from an Alarm using WebStation
  • Adding an Attachment to Multiple Alarms
  • Copying Attachments to Multiple Alarms
  • Removing Attachments from Multiple Alarms