earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Basic Functionality
12/2/2024

Mass Backup

Mass backup is a method of performing a manual, simultaneous backup of all the EcoStruxure BMS servers in the network, which is useful for capturing data at a critical point, such as prior to an upgrade. You can choose which EcoStruxure BMS servers you want to back up along with the type of data for each.

In smaller installations, a server group may include an Enterprise Server and one or more field servers. In larger installations, multiple server groups may include an Enterprise Server with a distinct set of field servers.

In an EcoStruxure BMS that has an Enterprise Central with attached Enterprise Servers, you can do a mass backup of all the Enterprise Servers.

 
action_zoom_plus_stroke Mass backup of an Enterprise Server and field servers
Figure: Mass backup of an Enterprise Server and field servers

You log on to the Enterprise Server to create a mass backup. For more information, see Backup Options Dialog Box .

  • Manual Backups
  • Backup
  • Synchronized Backups
  • Backup Options Dialog Box