earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Enterprise Central, Enterprise Server, Esmi Sense FDP
Functionalities: Alarms
12/2/2024

Multistate Alarms

​The multistate alarm monitors a variable and triggers the alarm if the variable is between the configured alarm range or equal to a single value. You can add several ranges or single values to trigger the alarm.

Note:
  • The trigger values and the monitored variable must be integer.

 
action_zoom_plus_stroke Multistate alarm triggers an alarm when the monitored variable goes inside the configured range or a single value.
Figure: Multistate alarm triggers an alarm when the monitored variable goes inside the configured range or a single value.

For example, you have a function block program with an output variable that generates integer values for different states. By using a multistate alarm, you can monitor a specific value or several value ranges.

You can configure multistate alarms using shunt variable and time delay. For more information, see Alarm Functions .

  • Alarm Types
  • Alarms Overview
  • Alarm Functions
  • Multistate Alarm Properties – Basic Tab
  • Creating a Multistate Alarm