earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: ​License Administrator, ​License Server
Functionalities: License Management
2/27/2025

Return Licenses Administrated by License Administrator

When you return a license administrated by License Administrator, the license is transferred from the License Server back to the License Activation Server.

When a license is returned, all the licenses that were activated in the same session are also returned. For example, if seven licenses are activated in the same activation transaction, a single license cannot be returned to the License Activation Server.

To activate the returned licenses again, use the entitlement ID that contains the returned licenses.

This flow describes the return transaction of licenses from a License Server to the License Activation Server.

 
action_zoom_plus_stroke Returning a license from License Server to the License Activation Server
Figure: Returning a license from License Server to the License Activation Server

Table: Returning Licenses from License Server to the License Activation Server

Number

Description

1

In the License Administrator, select the licenses to return.

2

The License Administrator returns the licenses to the License Activation Server.

Note:
  • All licenses that were activated in same transaction are returned to the License Activation Server.

  • Maintenance of Licenses Administrated by License Administrator
  • Removing Demo Licenses on License Administrator