Use the Create Object dialog to create and edit an object.
|
Component |
Description |
|
(Object type list) |
Select the type of object you want to create. For more information, see EcoStruxure Building Operation Objects . |
|
Name |
Type the name of the object. For more information, see Object Names . |
|
Prefix |
Type a label that is added in front of the object name. For more information, see Suffix and Prefix . |
|
Suffix |
Type a label that is added after the object name. For more information, see Suffix and Prefix . |
|
Path |
Enter the path to the location in the System Tree where you want to create the object. By default, the path to the selected folder or object in the System Tree is displayed. |
|
Description |
Type a description that explains what the object is used for. |
|
Next |
Click to use the wizard when you create the object. |
|
Create and edit |
Click to create the object. This option closes the Create object dialog and navigates to the object. |
|
Create |
Click to create the object and close the Create object dialog |