earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: User Management
12/2/2024

Panel Properties

Use the Panel properties to configure the properties of a panel.

 
action_zoom_plus_stroke Panel properties
Figure: Panel properties

Table: Panel Properties

Component

Description

Work area initial path

Enter the path, for example a graphical link, that points to the panel.

Show toolbars

Select Yes to show the toolbars of the panel.​

 
action_zoom_plus_stroke

Add

Click to add a pane component to the panel. For more information, see Create Object Dialog – Naming the Object Page .

 
action_zoom_plus_stroke

Edit

Click to edit a pane component. For more information, see Pane Properties .

 
action_zoom_plus_stroke

Remove

Click to remove a panel component.

  • Panel Components
  • Create Object Dialog – Naming the Object Page
  • General Information Properties – Basic Tab