earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: WebStation
Functionalities: Basic Functionality
10/30/2025

Basic Functions

WebStation has a many functions that help you work efficiently. You can search for and organize objects, and you can get help using the online help.

Log on to WorkStation or WebStation

You log on to WorkStation or WebStation to securely access the EcoStruxure BMS features.

For more information, see WebStation or WorkStation Login .

Regional Settings and Theme Settings

You can change regional settings and use different themes to adapt WebStation to your region and your screen.

For more information, see Regional Settings and Theme Settings .

Workspace

The workspace in WorkStation and WebStation is the area where you perform all tasks at your site, such as acknowledging alarms and viewing trend logs.

For more information, see Workspaces .

Search, Sort, and Filter

WebStation has features to help you in your daily work. For example, you can search for, sort, and filter objects.

For more information, see Search, Sort, and Filter .

Modify Values

You can change and force values using a graphic or the Properties pane. Using the Watch pane, you can dynamically monitor a value.

For more information, see Modify Values .

Help in WebStation

The EcoStruxure BMS Help provides you with information on how to handle and understand the system.

For more information, see Help in WebStation .

Security Configuration in WebStation

For security reasons, the default configuration for WebStation is, for example, not to allow external content to be embedded.

For more information, see Security Configuration in WebStation .

Disable Unnecessary Animations

WebStation supports disabling of unnecessary animations. The disabling can only be done in the operation system. To disable unnecessary animations, refer to your operation system. The disabling of unnecessary animations does not affect animated graphics, such as TGML graphics in WebStation.

  • Building Operation WebStation Overview
  • Workspaces
  • Regional Settings and Theme Settings
  • WebStation or WorkStation Login
  • Search, Sort, and Filter
  • Modify Values
  • Help in WebStation
  • Security Configuration in WebStation