You reinstall the Enterprise Server to replace your current installation with a fresh copy.
Ensure that you have a backup of the Enterprise Server data.
In Windows, disable any anti-virus program.
Double-click the Enterprise Server installation file to start the installation wizard.
Click Yes to confirm that you want to run the EcoStruxure Building Operation installation package.
The Enterprise Server Windows Service is automatically stopped.
Click Next .
In the License Agreement page, make sure that you agree with the End User License Agreement (EULA) and then click I Agree .
In the Installation Folder page, click Next .
Accept the database folder or browse to select another installation folder for the database and then click Next ..
The database folder path can contain up to 140 characters.
Click Next .
In the Installation Type page, select Uninstall current version before reinstalling .
Click Next .
In Communication Ports page, in the HTTP Port box, type the port number the Enterprise Server listens to when communicating through the Hypertext Transfer Protocol.
In the HTTPS Port box, type the port number the Enterprise Server listens to when communicating through the Hypertext Transfer Protocol Secure.
In the TCP Port box, type the port number the Enterprise Server listens to when communicating through the Transmission Control Protocol.
In the GraphDB Port box, type the port number the Enterprise Server uses to communicate with the Graph database that is used for semantic tagging.
In the SAML Authenticator port box, type the port number the SAML Authenticator uses.
Click Next .
In the Windows Service page, select Local system to run the Enterprise Server under the Local system account.
For security reasons, it is recommended that you run the Enterprise Server service under a custom Windows user account with limited permissions.
To run the Enterprise Server service under a custom Windows account, select Custom, enter the domain and user account names, click Verify Account to verify that the account exists, and then type the user account password.
To be able to log on to WebStation, the selected Windows user account has to have write permissions to C:\Program Files (x86)\Schneider Electric EcoStruxure\Building Operation X.X\Enterprise Server.
In the License Server Address box, type @ and then type the address to the License Server.
If the License Server uses a port other than the default port range 27000-27009, type the port number in front of @. For example, 567@localhost.
Use a semicolon to separate addresses to different License Servers.
Click Next .
Clear Enable semantics if you do not want to use semantics.
Click Next .
Clear Launch Cloud Agent Installer Wizard ... if you do not want to launch Cloud Agent Installer Wizard. You can launch Cloud Agent Installer Wizard later.
Click Next .
Revise the information on the Summary page and then click Install .
Click Uninstall to remove the Enterprise Server from your computer.
Click Close to confirm the uninstallation of the Enterprise Server.
Click Next.
Click Show details to follow the progress of the reinstallation.
Click Finish .
If you chosen to launch Cloud Agent Installer Wizard, follow the instructions.
In Windows, enable any anti-virus program.
In Windows, enable any anti-virus program.