earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Basic Functionality
12/2/2024

Remote Backup and Restore of Field Servers

When you log on to an Enterprise Server, you can perform remote backups of any field server in the system. Whenever a backup occurs on the field server, the system overwrites the locally stored file on the field server with the new backup file. The Enterprise Server then retrieves and stores this backup file in a separate directory on the computer that runs the Enterprise Server.

When you want to restore a field server, the system displays only the valid field server backup files that are stored on the Enterprise Server.

In the event that the backup file on the field server is damaged or lost, or not the one you want to use, you can select a valid backup file to restore the field server. The restore operation overwrites the locally stored field server backup file located on the field server with the selected backup file. For more information, see Restoring a Field Server from the Enterprise Server .

  • Manual Backups
  • Backup Sets
  • Restoring a Field Server from the Enterprise Server