earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WorkStation
Functionalities: Trends
12/2/2024

Removing a Trend Chart Series

You remove unused series from the trend chart.

Show More
action_close

Trend charts are a way to graphically present trend logs. A trend chart can contain one or more trend logs that are represented in the trend chart by lines or bars.

You can also add and remove trend logs from a trend chart. This makes it easy to compare different trend logs, for example the energy consumption compared to the average temperature.

 
action_zoom_plus_stroke Trend chart in WorkStation
Figure: Trend chart in WorkStation

Trend Chart Navigation in WorkStation

The trend chart contains a lot of tools for easy navigation in the chart. You can scroll or use the predefined settings to focus on the time span you want to see.

For more information, see Trend Chart Navigation in WorkStation .

Trend Chart Navigation in WebStation

The trend chart contains a lot of tools for easy navigation in the chart. You can scroll or use the predefined settings to focus on the time span you want to see.

For more information, see Trend Chart Navigation in WebStation .

Trend Chart Series in WorkStation

You can display the trend logs as trend log series in a trend chart in a number of ways. For example, you can change the color and weight of the trend log line, or display markers at the time where the trend log value was sampled.

For more information, see Trend Chart Series in WorkStation .

Trend Chart Series in WebStation

You can display the trend logs as trend log series in a trend chart in a number of ways. For example, you can change the color and weight of the trend log line, or display markers at the time where the trend log value was sampled.

For more information, see Trend Chart Series in WebStation .

Trend Chart Axes in WebStation

​A trend chart displays the records of a trend log or an extended trend log as a series.

For more information, see Trend Charts .

To remove a trend chart series
  1. In WorkStation, in the System Tree pane, select the trend chart from which you want to remove a series.

  2. On the Trend Chart , click the Series tab.

  3. In the Series area, right-click a series and select Remove series .

The selected series is now removed from the trend chart.

  • How Trend Logs Work
  • How Trend Charts Work
  • Trend Chart Event Icons
  • Opening a Trend Log List
  • Refreshing a Trend Log List
  • Changing the Color of a Trend Chart Series
  • Changing the Line Weight of a Trend Chart Series
  • Showing Markers in a Trend Log Series
  • Viewing Events in a Trend Chart
  • Hiding a Series in a Trend Chart
  • Changing the Display Order of a Trend Chart Series
  • Displaying Trend Log List Values as Decimals
  • Displaying Trend Log List Values as Bitstrings