earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Basic Functionality
12/2/2024

Restore Options Dialog Box

Use the Restore Options dialog box to select a backup set and the type of data that you want to restore. You can also import a backup set from a network storage location and restore the EcoStruxure BMS server, or duplicate an EcoStruxure BMS server from a backup set using Restore when you want to reuse configuration data from a backup set in a standalone field server.

 
action_zoom_plus_stroke Restore Options dialog box
Figure: Restore Options dialog box

Table: Restore Options Dialog Box

Component

Description

Name

Displays the name of the backup set for the selected EcoStruxure BMS server.

Created on

Displays the date the backup set was created.

Description

Displays a description of the backup set.

Server version

Displays the server version.

Server type

Displays the server type.

Configuration only

Select to restore only the configuration data and custom object type data. No historical data is restored.

All Data (Configuration and Historical)

Select to restore the historical data, configuration data, and custom object type data.

Import Backup Set

Click to import the backup set to an EcoStruxure BMS server. In a multi-server configuration, you can import both field server and Enterprise Server backup sets to the Enterprise Server.

Restore configuration with new IDs

Select to duplicate the configuration data from the imported backup set in the new standalone field server. The communication settings from the backup set will not be duplicated.

For more information, see Duplicate Field Server from a Backup Set .

  • Backup Set Storage and Protection
  • Backup Set Import from WorkStation
  • Backup Options Dialog Box
  • Backup and Restore Manager on the Enterprise Server
  • Restore Incomplete Due to Network Connectivity Loss
  • No Restore Files Display After Backup
  • Renamed Field Server Makes Backup Sets Unavailable
  • Duplicate Field Server from a Backup Set
  • Backup Set Text is Red