earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, Esmi Sense FDP
Functionalities: Basic Functionality
12/3/2024

Backup Rules Toolbar

Use the Backup rules toolbar to add, edit, or remove backup rules.

Button

Description

 
action_zoom_plus_stroke

Add backup rule

Click to open the Create Object wizard where you create a backup rule. For more information, see Creating a Backup Rule .

 
action_zoom_plus_stroke

Edit backup rule

Click to open the Backup rule dialog box where you modify a backup rule. For more information, see Editing a Backup Rule .

 
action_zoom_plus_stroke

Remove backup rule

Click to delete a backup rule. For more information, see Deleting a Backup Rule .

  • Creating a Backup Rule
  • Editing a Backup Rule
  • Deleting a Backup Rule