earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Trends
10/30/2025

Saving Current Trend Chart Settings

You save the trend chart settings if you want the trend chart to be displayed the same way the next time you open it.

Show More
action_close

Trend charts are a way to graphically present trend logs. A trend chart can contain one or more trend logs that are represented in the trend chart by lines or bars.

You can also add and remove trend logs from a trend chart. This makes it easy to compare different trend logs, for example the energy consumption compared to the average temperature.

You can print a trend chart.

 
action_zoom_plus_stroke A trend chart
Figure: A trend chart

Trend Chart Navigation

The trend chart contains a lot of tools for easy navigation in the chart. You can scroll or use the predefined settings to focus on the time span you want to see.

For more information, see Trend Chart Navigation in WorkStation .

How Trend Charts Series Works

You can display the trend logs as trend log series in a trend chart in a number of ways, for example, you can change the color and weight of the trend log line, or display markers at the time where the trend log value was sampled.

For more information, see Trend Chart Series in WorkStation .

Trend Charts

​A trend chart displays the records of a trend log or an extended trend log as a series. Variables can also be displayed in a trend chart, which is called a real-time plot. For more information, see Real-Time Plotting .

For more information, see Trend Charts .

To save current trend chart settings
  1. In WebStation, in the System Tree pane, open the trend chart.

  2. On the Trend Chart toolbar, click the Settings button

     
    action_zoom_plus_stroke
    .
  3. Change the settings to fit your preferences.

  4. On the Trend Chart toolbar, click Save.

  • Trend Chart Series in WebStation
  • How Trend Charts Work
  • Opening a Trend Chart
  • Trend Chart View