earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, FDP Server, WorkStation
Functionalities: Schedules
12/2/2024

Schedule Event Properties Dialog Box – Calculated Exception View

Use the Calculated Exception view in the Schedule Event Properties dialog box to schedule recurring exceptions.

 
action_zoom_plus_stroke Schedule Event Properties dialog box - Calculated exception view
Figure: Schedule Event Properties dialog box - Calculated exception view

Table: Schedule Event Properties Dialog Box – Calculated Exception View

Component

Description

Event type

Click Exception to display the exception types.

Exception type

Select Calculated for an exception type to apply to the schedule.

 
action_zoom_plus_stroke

Click to add a line to the Times and values box.

 
action_zoom_plus_stroke

Click to delete an entry from the Times and values box.

All Day

Select to create an all day event.

Name

Type a name for the event.

Priority

Select a priority number between 1 (highest priority) and 16 (lowest priority).

Year

Displays Any Year which is the default for the calculated exception view.

Month

Select a month for the exception event or Odd month , Even month , Any month .

Week of month

Select a week of the month for the exception event or First week , Second week , Third week , Fourth week , Last week , Any week .

  • First week – the first through the seventh day of the month. The second week is then considered day of month eight through fourteen and so on. Since the dates do not necessarily correspond to the first row of the calendar, they may include dates from both the first and second row of the calendar.

  • Fifth week – days 29 through 31 if they exist. It is always less than seven days and is non-existent in February except in a leap year.

  • Last week – the last seven days of the month. It differs from the Fifth wee k .

Week of month

Select a week of the month for the exception event or First week , Second week , Third week , Fourth week , Last week , Any week .

  • First week – the first through the seventh day of the month. Be aware that it does not necessarily correspond to the first row of the calendar since it may include dates from both the first and second row of the calendar.

  • Fifth week – days 29 through 31 if they exist. It is always less than seven days and is non-existent in February except in a leap year.

  • Last week – the last seven days of the month. It differs from the Fifth wee k .

Day of week

Select a day of the week. Setting the value to Any Day ensures consistency with the rest of the date specification, this is the recommended setting.

  • Exception Events in WorkStation