earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, Esmi Sense FDP
Functionalities: Basic Functionality
12/2/2024

Select Types Dialog Box

Use the Select types dialog box to select the object types you want to include in the search.

 
action_zoom_plus_stroke
Figure:

Table: Select Types Dialog Box

Component

Description

Object type tree

Select the object type to search for.

 
action_zoom_plus_stroke

Add type

Click to add the selected object type to the search.

 
action_zoom_plus_stroke

Remove type

Click to remove the selected object from to the search.

Selected object types

Displays the object types that are included in the search.

Find type

Type the name of the object type you want to include.

  • Search Overview
  • Search View Toolbar
  • Select Folder Dialog Box
  • Select Conditions Dialog Box