earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Enterprise Central, Enterprise Server, Esmi Sense FDP, WorkStation
Functionalities: Trends
12/2/2024

Showing Trend Chart Grid Lines

You show the trend chart grid lines on the x-axis and the y-axis to make the chart easier to read.

Show More
action_close

Use the Axes tab to configure the properties of the chart axes.

 
action_zoom_plus_stroke Axes tab
Figure: Axes tab

Table: Axes Tab

Component

Description

Time mode

​Select the time mode of the x-axis.

Start time

Enter the absolute start time when Time mode is set to Absolute. This time is the leftmost point of the x-axis.

End time

Enter the absolute end time when Time mode is set to Absolute (start time and end time) . This time is the rightmost point of the x-axis.

Time span

Type the relative time span of the x-axis when Time mode is set to Relative (to current time) . The rightmost point of the x-axis is the current time.

Time zone

Select time zone for the trend chart. The time zone is the displayed time perspective of the trend log.

Show grid lines

Select to show horizontal grid lines.

Auto scale left y-axis

Select to activate auto scale. The scale of the left Y-axis adapts itself to the displayed series.

Left y-axis minimum

Type the minimum value of the left y-axis.

Left y-axis maximum

Type the maximum value of the left y-axis.

Show left grid lines

Select to show grid lines on the left y-axis.

Auto scale right y-axis

Select to activate auto scale. The scale of the right y-axis adapts itself to the displayed series.

Right y-axis minimum

Type the minimum value of the right y-axis.

Right y-axis maximum

Type the maximum value of the right y-axis.

Show right grid lines

Select to show grid lines on the right y-axis.

To show trend chart grid lines
  1. In WorkStation, in the System Tree pane, select the trend chart you want to configure.

  2. On the Trend Chart toolbar, click the Open trend chart settings button

     
    action_zoom_plus_stroke
    .

  3. Below the Time zone box, select Show grid lines to show grid lines originating from the x-axis scale.

  4. Select Show left grid lines or Show right grid lines to show grid lines originating from the y-axis scale.

  5. Click OK .

Grid lines are now shown in the trend chart. Repeat the procedure to hide the grid lines.

 
action_zoom_plus_stroke

  • Trend Chart Axes
  • Trend Charts
  • Trend Chart Settings Dialog Box – Axes Tab
  • Trend Chart Event Icons