earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Enterprise Central, Enterprise Server, FDP Server, WorkStation
Functionalities: Basic Functionality
12/2/2024

Simple Search

arrow1_rotationWildcard Search arrow1_rotationSearch Result List

Use Simple Search to search for object names.

Use the Search view to search for names of properties. For more information, see Searching for Objects or Properties .

 
action_zoom_plus_stroke Simple search toolbar and search result list
Figure: Simple search toolbar and search result list

Wildcard Search

When searching, you use wildcards to substitute characters or combinations of characters.

​Search supports three wildcards:

  • ​Asterisk (*) represents any combination of characters including white space. * must be used if the text string you search for contains white space. For example, if you want to search for object names as "temperature setpoint" or "setpoint office" make sure that you use "*" in the end or in the beginning of the word "setpoint".

  • ​Question mark (?) represents any single character.

  • Square brackets “[]” search for all characters that stands inside the brackets.

​For example, if you want to find all objects and properties containing the word “Temperature”, you start the search with an asterisk so that the search includes all hits on objects like “Outside Air Temperature” where the asterisk represents the words before "Temperature", in this case, “Outside Air”. You also have to end the search text with an asterisk to include objects like “Temperature Alarm” where the asterisk represents the word after "Temperature", in this case “Alarm”. ​

If you search on [a,b]*, you find all objects that begins with an a or a b​.

You can also search on objects that start with numbers using square brackets. For example, a search on [0-9]* finds all objects that starts with a number. A search on [1,2,3]* finds all objects that starts with 1, 2, or 3.

Note:

​The Search box can never be empty. To perform a search, you have to enter something in the Search box. If you want to search for all objects in a folder, enter an asterisk (*).

Search Result List

The search result list can be sorted and grouped in a number of ways. You can also add and remove columns from the list. Using Properties , you can also open the properties for all objects in the list.

  • Search Overview
  • Search Toolbar
  • Searching for Objects Using Simple Search