earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WorkStation
Functionalities: Basic Functionality
12/2/2024

Status Bar

Use the Status bar to view information on the following items:

  • connectivity status

  • security certificates

  • which EcoStruxure BMS server the user is logged on to

  • the name of the logged on user account

  • which domain the user is logged on to

  • whether or not database mode is active

  • the current language

  • the measurement system

 
action_zoom_plus_stroke Status bar
Figure: Status bar

Component

Description

 
action_zoom_plus_stroke

Indicates that the security certificate is valid.

 
action_zoom_plus_stroke

Indicates that the security certificate cannot be validated.

 
action_zoom_plus_stroke

Connected to

Indicates that WorkStation is connected to the EcoStruxure BMS server.

 
action_zoom_plus_stroke

Trying to connect to

Indicates that WorkStation is disconnected from the EcoStruxure BMS server and trying to connect.

User account

Displays the account you are currently using.

Domain

Displays the domain you are logged on to.

 
action_zoom_plus_stroke

Database mode

Indicates that database mode is active. For more information, see Database Mode .

Current language

Displays the current display language of the system in the drop-down menu beside the user account.

Measurement system

Displays the selected measurement system for the system in the drop-down beside the user account.

  • Workspaces
  • WorkStation Workspace
  • Database Mode