earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, Esmi Sense FDP
Functionalities: Localization
12/2/2024

Time Zone Properties – Zone Info Tab

Use the Zone Info tab to configure the time zone settings ​or establish a lead and shadow relationship on EcoStruxure BMS servers.

 
action_zoom_plus_stroke Zone info tab
Figure: Zone info tab

Table: Zone Info Tab

Component

Description

Time zone

​Select the time zone the EcoStruxure BMS server belongs to.

Use custom time zone

Select Enabled to configure and use a custom time zone.

Lead object

​Enter the object that acts as the lead for this object.

Description

Type a description or name for the customized time zone DST settings.

GMT offset - hours

Select the time difference the time zone has from GMT in hours.

GMT offset - minutes

Select the time difference the time zone has from GMT in minutes.

Daylight saving time

Select Enable if the custom time zone uses daylight saving time.

DST Delta (Minutes)

​Select the time adjustment, in minutes, for the daylight saving time.

DST Start Month

Select the month that daylight saving time starts.

DST Start Week

​​Select the week of the month that daylight saving time starts.

DST Start Day

Select the day of the week that daylight saving time starts.

DST Start Hour

Select the hour of the day that daylight saving time starts.

DST Start Minute

Select the minute of the hour that daylight saving time starts.

DST End Month

Select the month that daylight saving time ends.

DST End Week

Select the week that daylight saving time ends.

DST End Day

Select the day of the week that daylight saving time ends.

DST End Hour

Select the hour of the day that daylight saving time ends.

DST End Minute

Select the minute of the hour that daylight saving time ends.

  • Time Zone Settings Synchronization
  • Time and Time Zone Overview
  • Date & Time View
  • Time Zone Properties – Basic Tab