earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: WorkStation
Functionalities: Trends
12/2/2024

Trend Log List Display

A trend log list can be displayed in a number of ways.

You can present the values in the trend log as decimals or as bitstrings. You can hide or display events in a trend log list to make the reading easier. Events that have a value or comment cannot be hidden and are always displayed.

The settings can be saved so that the trend log list is displayed in the same way the next time you open it.

  • Trend Log Lists in WorkStation
  • Displaying or Hiding Events in a Trend Log List
  • Displaying Trend Log List Values as Decimals
  • Displaying Trend Log List Values as Bitstrings
  • Saving a Trend Log List Setting