earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Trends
12/2/2024

Trend Log List Event Icons

Use the trend log list event icons to get information on different trend log events.

Table: Trend Log List Event Icons

Icon

Description

 
action_zoom_plus_stroke

Log was started

Indicates that the trend log started recording values.

 
action_zoom_plus_stroke

Log was stopped

Indicates that the trend log stopped recording values.

 
action_zoom_plus_stroke

The log is not configured

Indicates that the trend log is not correctly configured or preferences are missing, so the trend log cannot start recording values.

 
action_zoom_plus_stroke

A log value was missed

Indicates that one or more records were missed due to interrupted communication, hardware failure, or software failure.

 
action_zoom_plus_stroke

The log configuration was updated

Indicates that the settings of the trend log were updated. The change is described in the comment column of the table.

 
action_zoom_plus_stroke

Record was added

Indicates that a record was manually added.

 
action_zoom_plus_stroke

Record was edited

Indicates that a record was manually edited.

 
action_zoom_plus_stroke

Record was commented

Indicates that a log record was commented. The comment is displayed in the ToolTip of the event and in the comment column of the table.

 
action_zoom_plus_stroke

Log was cleared

Indicates that a trend log was cleared.

 
action_zoom_plus_stroke

Meter was changed

Indicates that the meter was changed or that the settings were configured.

This event symbol only applies to the meter trend log.

 
action_zoom_plus_stroke

System clock changed

Indicates that the system date or time, where the trend log is located, has been changed. For more information, see Time and Time Zone Overview .

 
action_zoom_plus_stroke

Override

Indicates that the recorded value is overridden by the hardware and is not the measured value.

Forced

Indicates that the recorded value is forced by the software and is not the measured value.

 
action_zoom_plus_stroke

Log database restored

Indicates that the log database has been restored and that, when the log restarts, there can be a time gap in the log series.​

 
action_zoom_plus_stroke

Log reset by extended log

Indicates that the commands from the extended trend log have been cleared from the trend log.

  • Trend Log Lists
  • Time and Time Zone Overview
  • Time Zone Modes in a Trend Log List
  • Interrupted Series in the Trend Chart
  • Illogical or Missing Records in the Trend Log List
  • Trend Log List View