earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, Esmi Sense FDP
Functionalities: Trends
12/3/2024

Create Extended Trend Log Wizard – Configure Extended Trend Log Page

Use the Configure Extended Trend Log page to configure the settings of the extended trend log.

 
action_zoom_plus_stroke Configure Extended Trend Log page
Figure: Configure Extended Trend Log page

Table: Configure Extended Trend Log Page

Component

Description

Monitored trend log

​Enter the trend log that you want to transfer records from.

Smart log

​Select True to optimize the transfer of the monitored trend log to the extended trend log.

Threshold

​Select the ​percentage threshold at which the trend log transfers its records to the extended trend log.

Maximum transfer interval

Select the maximum length of time that can pass between transfers from the monitored trend log to the extended trend log.

Transfer trigger variable

Enter a trigger variable to force a transfer of all records from the trend log to the extended trend log, for example, to generate a complete report. For more information, see Extended Trend Logs .

Log size

Select the number of records to store before old records are overwritten including internal records generated by the trend.

Available trend storage

Displays the trend storage usage and the number of records left in the trend storage.

Include in reports?

Select True to include the extended trend log data in reports.

  • Extended Trend Logs
  • Extended Trend Log Properties – Basic Tab
  • Log Record Storage
  • Create Object Dialog – Naming the Object Page
  • Records Are Not Transferred to the Extended Trend Log