earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, Esmi Sense FDP
Functionalities: Trends
12/2/2024

Actions Menu – Activation Submenu

Use the Activation submenu to enable, disable, or clear a trend log.

 
action_zoom_plus_stroke The trend log Actions menu, Activation submenu
Figure: The trend log Actions menu, Activation submenu

Table: Activation Submenu

Command

Description

Enable trend log

Click to enable the trend log. The trend log starts when the start condition is fulfilled.

Disable trend log

Click to disable the trend log and stop all recording activity.

Clear trend log

Click to clear all the records from the trend log.

Force transfer

Click to manually forces the transfer of records to the extended trend log.

  • Extended Trend Logs
  • Actions Menu