earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Localization
6/2/2025

Select Unit Dialog Box

Use the Select Unit dialog box to define the unit and metric prefix of a value.

 
action_zoom_plus_stroke Select Unit dialog box
Figure: Select Unit dialog box

Table: Select Unit Dialog Box

Component

Description

Recent

Displays a list of the 12 most recently selected units with prefix.

Quick filter

Type the name of the category or unit you are searching for. For more information, see Quick Filter .

More units

Select the category and unit of the value. For more information, see Units .

Prefix

Select the prefix of the unit

Selected unit

Displays the defined unit with prefix.

Note:

When selecting a unit, you can either select it from the Recent list, or in the More units section.

  • Regional and Language Overview
  • Quick Filter
  • Units
  • Metric Prefixes
  • Precision Format
  • WorkStation does not Display Correct Values