earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, Esmi Sense FDP
Functionalities: User Management
12/2/2024

User Account – Software Permissions Tab

Use the Software Permissions tab to enter individual path permissions for a user account.

Note:
  • To simplify the task of administering software permissions, it is recommended that you assign software permissions to user account groups rather than user accounts.

 
action_zoom_plus_stroke Software permissions tab
Figure: Software permissions tab

Table: Software Permissions Tab

Component

Description

 
action_zoom_plus_stroke

Add

Click to add a path to the list of paths the user account can access.

 
action_zoom_plus_stroke

Add System

Click to add the the system's top level path.

Path

Displays the paths that have been defined for the user account.

Permissions

Click to assign a permission level to a path you have selected. For more information, see Software Permissions Rules Management .

Properties

The access to the Property Permissions dialog box where you define the level of permissions to object properties for the user account.

 
action_zoom_plus_stroke

Property Permissions

Click to access the Property Permissions dialog box. For more information, see Property Permissions .

Relative path permissions

Browse to a folder structure to grant a specific set of permissions to a user account to all the folders accessible in a predefined path and its folder structure.

Owner

Displays the user account the path has been added to. Owner can be one or more user account groups the user account is a member of or the user account.

 
action_zoom_plus_stroke

Add

Click to add a path to the type permission object the user account group can access.

 
action_zoom_plus_stroke

Delete

Click to remove a path from the list of paths the user account can access. For more information, see Confirm Delete Dialog Box .

Type permission

Displays the type permissions that have been defined for the user account2020.

  • User Accounts and User Account Groups
  • Software Permissions
  • Software Permissions Rules Management
  • Property Permissions
  • Confirm Delete Dialog Box
  • Property Permissions Dialog Box