earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WorkStation
Functionalities: Basic Functionality
12/2/2024

View Menu

Use the View menu to display or hide Workspace components.

 
action_zoom_plus_stroke The View menu
Figure: The View menu

Command

Description

Forward

​Click to go forward to a view you have visited before in the selected window.

Back

​Click to go back to a view you have visited before in the selected window.

Workspaces

Use the Workspaces submenu to switch to another workspace. For more information, see View Menu – Workspaces Submenu .

Save workspace layout

Click to save workspace layout changes you have made to the workspace on the local computer. For more information, see Workspace Components and Customization .

Reset workspace layout

Click to reset workspace layout to the default workspace layout on the local computer. For more information, see Workspace Components and Customization .

Set the current workspace as default

Click to set the current workspace layout as the default workspace on the local computer. For more information, see Workspace Components and Customization .

Toolbars

Use the Toolbars submenu to hide or display the menus in WorkStation. For more information, see View Menu – Toolbars Submenu .

Watch

Select to display the Watch pane where you monitor variables. For more information, see Watch Pane and Watch View .

System Tree

Select to display the System Tree where you can see and work with all objects in your system. For more information, see System Tree Pane .

Events

Select to display the Events pane where you inspect events. For more information, see Events Pane and Event View Customization .

Alarms

Select to display the Alarms pane where you handle alarms. For more information, see Alarms Pane and Alarm View Customization .

Full screen

Select to display the selected window in the work area in full screen mode. For more information, see Using Full Screen Mode .

  • History Bar
  • View Menu – Workspaces Submenu
  • Workspace Components and Customization
  • View Menu – Toolbars Submenu
  • Watch Pane and Watch View
  • Events Pane and Event View Customization
  • Alarms Pane and Alarm View Customization
  • Using Full Screen Mode