earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, Esmi Sense FDP
Functionalities: User Management
12/2/2024

Workspace Wizard – Pane Configuration Page

Use the Pane configuration page to determine the layout of the component you are adding to the workspace.

 
action_zoom_plus_stroke Pane configuration page
Figure: Pane configuration page

Table: Pane Configuration Page

Component

Description

Show toolbar

Select No to hide the component toolbar.

Default dock position

Select a default dock position in the workspace for the component.

Default visibility

Select Hidden to hide the component.

Display name

Type the pane name that is to be displayed. Display name is available only in WorkStation.

Initial path

Click to change the location of the component. For more information, see Workspace Wizard – Workspace Configuration Page .

  • Workspace Components and Customization
  • Create Object Dialog – Naming the Object Page
  • Workspace Wizard – Workspace Configuration Page