earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WorkStation
Functionalities: Basic Functionality
12/2/2024

WorkStation Toolbar

Use the buttons on the WorkStation toolbar for easy access to commands you use frequently.

Table: WorkStation Toolbar

Button

Description

 
action_zoom_plus_stroke

Workspace

Click to open the Workspace menu where you can select a workspace.

 
action_zoom_plus_stroke

Control Panel

​​Click to open the Control Panel where you get access to some of the most used administration functions, such as alarms, domains, user accounts, backup and archiving, and engineering. For more information, see Control Panel Tab .

 
action_zoom_plus_stroke

New

​Click to open the New submenu where you create new objects. For more information, see File Menu – New Submenu .

 
action_zoom_plus_stroke

Open in New

​Click to open the selected object in a new tab in the work area.

 
action_zoom_plus_stroke

Save

Click to save changes.

 
action_zoom_plus_stroke

Cut

​Click to cut the selected objects. The objects are placed on the clipboard.

 
action_zoom_plus_stroke

Copy

​Click to copy the selected objects. The objects are placed on the clipboard.

 
action_zoom_plus_stroke

Paste

​Click to paste a copied or cut object.

 
action_zoom_plus_stroke

Delete

​Click to open the Confirm delete dialog box where you delete the selected object. For more information, see Confirm Delete Dialog Box .

 
action_zoom_plus_stroke

Cancel

​Click to cancel the latest command.

 
action_zoom_plus_stroke

​Refresh

​​Click to refresh the selected object or workspace.

 
action_zoom_plus_stroke

Print

​Click to print the selected object.

 
action_zoom_plus_stroke

Help

Click to open the EcoStruxure BMS help.

  • Workspaces
  • File Menu