earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: User Management
10/30/2025

Domain Properties

Use the Domain properties to configure the properties of a domain.

 
action_zoom_plus_stroke Domain properties
Figure: Domain properties

Table: Domain Properties

Component

Description

Maximum logon attempts

Select the maximum number of failed logon attempts that a user can make before WorkStation is temporarily locked.

Password

Type the password EcoStruxure BMS servers ​internally use to enhance the EcoStruxure BMS server communication security in the domain.

Confirm Password

Type the password EcoStruxure BMS servers ​internally use to enhance the EcoStruxure BMS server communication security in the domain.

Windows domain name

Type the name of the Windows domain where the Windows Active directory is located from which you want to map user account groups. For more information, see Windows Active Directory User Groups .

  • Domains
  • General Information Properties – Basic Tab
  • EcoStruxure BMS Server Communication