earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Basic Functionality
10/30/2025

Logging Off WebStation

You log off WebStation so that unauthorized personnel cannot tamper with your settings.

Show More
action_close

You log on to WorkStation or WebStation to securely access the EcoStruxure BMS features.

Log on to WorkStation

You log on to WorkStation with your current Windows credentials, as another Windows user, or as an EcoStruxure BMS user. Your system administrator decides which type of user you log on as. ​

To log on to WorkStation using an EcoStruxure BMS account, you need to know the following account information:

  • User name

  • Password

  • Domain

  • EcoStruxure BMS server

To log on to WorkStation using a Windows account, you need to know the EcoStruxure BMS server.

The account information for both the EcoStruxure BMS account and the Windows account is provided by the system administrator.

Important:

​​Ensure that you have a working and available WorkStation license. A working license is required to log on to WorkStation. For more information, see EcoStruxure Building Operation Software Licensing Installation and Location .

Remember me on this computer

For a faster log on in Workstation, use the Remember me feature to automatically fill in your user name, password, domain and server. Both BMS users and Windows users can use the Remember me feature.

Add a display name of the server address

When you log on to a new server, its IP address is added to the server list. You can add a display name of the server address to make it easier to find your server in the list.

Log on to WebStation

To log on to WebStation, you need to know the following account information:

  • User name

  • Password

  • Domain

  • EcoStruxure BMS server

The account information for your account is provided by the system administrator.

To log off WebStation
  • In WebStation, on the Settings menu, click Options and then click Log off .

  • Log on to WorkStation or WebStation
  • Building Operation WebStation Window
  • Logging On to WebStation
  • Changing Your Password