earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WorkStation
Functionalities: Basic Functionality
10/30/2025

Switching Workspaces

You switch workspaces when you want to use another workspace, such as one with predefined functionality.

Show More
action_close

The workspace in WorkStation and WebStation is the area where you perform all tasks at your site, such as acknowledging alarms and viewing trend logs.

The workspace is made up of different components, such as panes, lists, and views. These components can be configured in a number of different ways. You can hide or display components and create and save your own workspace. You can also reset the workspace layout to the default layout for the user group your user account belongs to.

WebStation uses cookies to remember your workspace when you log off. When you log on again, you get the workspace you used when you logged off. If you clear your web browser, you will regain the default workspace.

Some objects have specific views in WorkStation and WebStation:

  • Alarms

  • Documents

  • Graphics (TGML)

  • Events

  • Trend Charts

  • Trend Log Lists

  • Schedules

  • Calendars

  • Watch

When you open an object that does not have a specific view, the Properties dialog box for that object is displayed.

Panels

Panels are a way to create workspaces that display two or more components in the EcoStruxure BMS software, for example graphics, trend charts, trend list, and alarm views.

For more information, see Panels .

Favorite Pages

You can add pages that you often visit as favorite pages. This makes the favorite pages more accessible.

For more information, see Favorite Pages .

External Contents

External contents, such as web pages, cannot be opened inside WebStation for security reasons.

To switch workspaces
  • In WorkStation, on the View menu, point to Workspaces , and then click the workspace you want to switch to.

  • Workspaces
  • WebStation or WorkStation Login
  • Logging on to WorkStation as an EcoStruxure Building Operation User
  • Logging on to WorkStation as another Windows User
  • Saving Log On Details
  • Selecting a Default Workspace
  • Logging Off WorkStation
  • Exiting WorkStation
  • Changing Your Password