earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Basic Functionality
10/30/2025

Time Stamp Value Properties

Use the Time Stamp Value properties dialog box to view or configure a time stamp value.

 
action_zoom_plus_stroke Time stamp value
Figure: Time stamp value

Table: Time Stamp Value

Property

Description

Value

Click the Configure button

 
action_zoom_plus_stroke
to select a reference. The value is read-only when selected.

Formatted timestamp

Displays a time stamp calculated from Localization and Custom time zone in the configured Time stamp format .

Timestamp format

Configure timestamp format.

Localization

Select Server time zone to display Formatted timestamp in the server time zone.

Select Custom time zone to display Formatted timestamp in a custom time zone.

Custom time zone

Select a custom time zone. If Server time zone is selected in Localization , Custom time zone is ignored.

  • General Information Properties – Basic Tab
  • References Tab
  • Creating an EcoStruxure BMS Server Value