earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebStation
Functionalities: Schedules
12/5/2025

Schedule Event Properties Dialog Box – Calculated Exception View

Use the Calculated Exception View in the Schedule Event Properties dialog box to schedule recurring exceptions.

 
action_zoom_plus_stroke Schedule event properties dialog box – Calculated 				exception view
Figure: Schedule event properties dialog box – Calculated exception view

Table: Schedule Event Properties Dialog Box – Calculated Exception View

Component

Description

All Day

Select to create an all day event.

Value

Enter a value for the exception event.

At

Enter the start time for the exception event.

Until

Enter the end time for the exception event.

Exception name

Type a name for the event.

Exception priority

Select a priority number between 1 (highest priority) and 16 (lowest priority).

Event type

Select Calculated .

Month

Enter the month when the calculated exception event occurs.

Week of month

Enter the day of month when the calculated exception event occurs.

Select a week of the month for the exception event or First week , Second week , Third week , Fourth week , Last week , Any week .

  • First week – the first through the seventh day of the month. The second week is then considered day of month eight through fourteen and so on. Since the dates do not necessarily correspond to the first row of the calendar, they may include dates from both the first and second row of the calendar.

  • Fifth week – days 29 through 31 if they exist. It is always less than seven days and is non-existent in February except in a leap year.

  • Last week – the last seven days of the month. It differs from the Fifth week .

  • Second to last week – any of the 7 days prior to the last 7 days of this month.

  • Third to last week – any of the 7 days prior to the last 14 days of this month.

  • Fourth to last week – any of the 7 days prior to the last 21 days of this month.

Day of week

Enter the day of week when the calculated exception event occurs.

  • Exception Events in WebStation
  • Schedule Event Properties Dialog Box – Weekly View
  • Schedule Event Properties Dialog Box – Single Date Exception View
  • Schedule Event Properties Dialog Box – Date Range Exception View
  • Schedule Event Properties Dialog Box – Calendar Reference View