earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: WorkStation
Functionalities: Basic Functionality
10/30/2025

User Experience

arrow1_rotationWorkspaces arrow1_rotationDifferent Layouts Using Panes arrow1_rotationWorkStation Shortcut keys arrow1_rotationWindows

The Work area in the EcoStruxure Building Operation user interfaces may vary depending on how it is set up. A typical EcoStruxure Building Operation workspace contains panes and views.

Workspaces

The workspace in WorkStation and WebStation is the area where you perform all tasks at your site, such as acknowledging alarms and viewing trend logs.

For more information, see Workspaces .

Different Layouts Using Panes

A pane is a separate area in the workspace. You use panes to carry out commands, navigate the system or display information. Panes can be moved, hidden, closed, and repositioned.

For more information, see Different Layouts Using Panes .

WorkStation Shortcut keys

To ease the daily operation, you can use shortcut keys to most of the commands inWorkStation.

For more information, see Keyboard Shortcuts for WorkStation .

Windows

You can navigate between the available open windows in the Work area. The windows you can select using the Window menu are represented by tabs in the Work area.

For more information, see Window Menu .

  • WorkStation Overview
  • Workspaces
  • Different Layouts Using Panes
  • Keyboard Shortcuts for WorkStation
  • Window Menu