earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: WebStation
Functionalities: Trends
12/2/2024

Trend Chart Axes in WebStation

The x-axis of the trend chart represents time. The time span of the axis can be set with a fixed start and end time or with an end time relative to the present time. The axis can be quick-scaled to show the last hour, last day, last month, or last year​.

 
action_zoom_plus_stroke Absolute time span and relative time span, schematic
Figure: Absolute time span and relative time span, schematic

The y-axis refers to the measurement unit that the variable represents. The scale of the y-axis can be set manually or by auto scale. You can configure the trend chart to present series on one y-axis or two y-axes, one to the left and one to the right. Use two y-axes to present series with different ranges in the same trend chart.

 
action_zoom_plus_stroke One y-axis and two y-axes, schematic
Figure: One y-axis and two y-axes, schematic

To make reading easier, grid lines can be shown in the trend chart. Grid lines can be shown in both the x- and y-direction, independent of each other.

 
action_zoom_plus_stroke Grid lines, schematic
Figure: Grid lines, schematic
  • Trend Charts
  • How Trend Charts Work
  • How Trend Logs Work
  • Trends Overview
  • Trend Chart View
  • Trend Chart Toolbar
  • Trend Chart Settings Dialog Box – X Axis Tab
  • Configuring the X-axis with a Relative Time Span
  • Configuring the X-axis with an Absolute Time Span
  • Showing Trend Chart Grid Lines
  • Manually Configuring the Y-Axis Scale
  • Automatically Configuring the Y-axis Scale