earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: WebStation
Functionalities: Schedules
12/17/2024

Calendars in WebStation

arrow1_rotationCalendar Editor Overview arrow1_rotationCalendar Events

A calendar is a list of dates. The calendar provides the schedule with the dates when the exception events shall occur. To save time, you can reference a single calendar rather than entering several exception events in a schedule.

 
action_zoom_plus_stroke Exception events in a calendar
Figure: Exception events in a calendar

Many schedules can make a reference to the calendar. You can define the group of dates once rather than over and over again in multiple schedules, a potentially tedious task if your building control system contains many schedules.

Calendar Editor Overview

You use the Calendar Editor to specify dates of exception events in a calendar. You can add and remove single dates. By using a calendar, you specify all the exception events only one time, rather than in each schedule. The calendar is then referenced to each of the schedules and all exception dates are automatically designated in the schedules.

For more information, see Calendar Editor Overview .

Calendar Events

You specify a single date in a calendar. A date is an entry that occurs once in the calendar.

  • Date: a specific date

For more information, see Calendar Events .

  • How Schedules Work in Fire Operation
  • Calendar Editor Overview
  • Calendar Events
  • Exception Events in WebStation