earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Specifications

Specifications


Products: Enterprise Server
Functionalities: Engineering
12/4/2024

Enterprise Server

arrow1_rotationIntroduction arrow1_rotationFeatures arrow1_rotationSpecifications
 
action_zoom_plus_stroke Enterprise Server
Figure: Enterprise Server

Introduction

An EcoStruxure BMS server is the core of the system and performs key functionality, such as control logic, trend logging, and alarm supervision. The Enterprise Server collects site-wide data for aggregation and archiving, and serves as a single point of administration through WorkStation or WebStation for the EcoStruxure BMS, Schneider Electric’s intelligent Building Management System.

Features

The Enterprise Server is a central point in the EcoStruxure BMS architecture from which users can configure, control, and monitor the system.

Semantics

Enterprise Server and Enterprise Central come with built-in support for modelling of the “digital twin” of the building, site, campus, and region using Brick Schema. WorkStation and WebStation provide enhanced human understandability through the additional context that is given to alarms and points through the “digital twin”. The required graph database is included in the installation packages. WorkStation can be used to create the model, or it can be imported using the graph database user interface.

Networking powerhouse

The Enterprise Server can run multiple control programs using a variety of protocols. It can manage alarms, users, schedules, and trend logs. Data from the Enterprise Server can be delivered directly to the user or to other EcoStruxure BMS servers and field devices throughout the site or enterprise.

Global view of the system

The entire site, including all of the field servers and their associated devices, can be accessed and configured through the Enterprise Server.

This overview of the site provides easier mass change engineering and data analysis. The Enterprise Server also aggregates the event and alarm data from all its associated field servers. Trend logs can be aggregated through the use of extended trend logs.

Text and graphics-based programming tools

Unique to the industry, the EcoStruxure BMS servers have both Script and Function Block programming options. This flexibility helps assure that a suitable programming method can be selected for the application.

Centralized alarms and data management

Alarms from multiple devices throughout the site, including field servers, are collected by the Enterprise Server for centralized logging, display, and management. Users can also view event logs and trend logs from multiple servers.

The Enterprise Server hosts the historical and configuration databases. These databases store current information, including trends, alarms, user activity, and property information. Alarms can trigger email, SNMP, file, or client notifications, which can include alarm, point value, or trend log data. Notifications can also be triggered periodically by schedules or other binary values.

EcoStruxure BMS servers can be configured to automatically store all historical data, trend log data, event log and audit trail data, in an external database. If data needs to be available for longer periods of time, an external log storage can be incorporated into the EcoStruxure BMS without the need for extensive engineering work. The supported databases are TimescaleDB, which is built on PostgreSQL, and Microsoft SQL Server. The data in the external log storage is available natively to the viewers built into the EcoStruxure Building Operation clients and to the built-in reporting functionality.

You can use the powerful Log Processor functionality for custom processing of trend data for viewing in charts, dashboards and for inclusion in reports. The Log Processor enables advanced calculations on one or multiple trend logs and point values.

Examples of advanced calculations:

  • Energy usage normalization

  • Virtual submeters and summaries

  • Calculation of Mean Kinetic Temperature

  • Unit conversions

  • Average, maximum, and mini m um over custom periods

The output of the Log Processor can be saved in the database, including the External Log Storage or calculated automatically on demand.

Selected trend logs and the event log can be sent to AVEVA PI System directly without the need for intermediate storage or specialized PI System connectors.

Reporting

The EcoStruxure BMS servers provide built-in functionality for basic reporting that can deliver reports in any text format and XLSX, without any dependencies to other external software. Reports for XLSX can be enriched by using advanced functionality such as formulas, conditional formatting, charts and sparklines.

Reports can be generated on schedule, on an alarm event or other custom conditions, and you can get the output delivered via email or written to file.

Using Enterprise Server and Enterprise Central, reports can be converted to PDF, and you can elevate the data security and traceability even further by using the optional add-on for automatically signing PDF reports with a digital certificate upon generation. This validates that the content has not been altered after the report was generated.

Authentication and permissions

An EcoStruxure BMS provides a powerful permission system that is easy to manage, flexible, and adapts to all kinds of system sizes. The permission system provides a high standard of authentication. Authentication is done against the built-in user account management system , against Windows Active Directory Domains , or via SAML 2.0 single sign-on . The built-in account management system allows an administrator to establish password policies that meet stringent cybersecurity guidelines. When Windows Active Directory or SAML 2.0 authentication is used, the administration costs are lower because users do not have to be managed in multiple directories.

Advanced activity log

It is important to log more than basic activity. In an EcoStruxure BMS, every action is logged with a timestamp, the user who performed the action, and the values that were changed.

WorkStation/WebStation interface

Through any client, the user experience is similar regardless of which EcoStruxure BMS server the user is logged on to. The user can log directly on to an Enterprise Server to engineer, commission, supervise, and monitor the field servers with their attached Central IO modules, field controllers, and other field devices. For more information, see the WorkStation and WebStation specification sheets.

Open building protocol support

One of the cornerstones of the EcoStruxure BMS is support for open standards. The Enterprise Server can natively communicate with some of the most popular standards for buildings: BACnet (including BACnet/SC), OPC UA Client, LonWorks, and Modbus.

Native BTL-listed BACnet support

The Enterprise Server communicates directly to BACnet/IP networks. The Enterprise Server is BTL-listed as a BACnet Building Controller (B-BC), the most advance BACnet device profile, and as a BACnet Operator Workstation (B-OWS). This capability provides access to the full range of BACnet devices from Schneider Electric and other vendors. See the BTL Product Catalog for up-to-date details on BTL listed software revisions on BACnet International's home page. The Enterprise Server can also serve as a BACnet Broadcast Management Device (BBMD) to facilitate BACnet systems that span multiple IP subnets.

BACnet/SC (Secure Connect) support

The Enterprise Server and field servers support BACnet/SC applications as a BACnet/SC node, hub, and router. This allows the Enterprise Server and field servers to be in BACnet/SC networks and support applications that connect BACnet/IP or MS/TP networks with BACnet/SC networks. A major benefit of BACnet/SC is that it allows more secure transport of BACnet traffic and information between BACnet/SC devices over private and public networks without the need for BBMDs, VLANs, and VPNs, because the BACnet/SC protocol uses WebSocket technology and TLS 1.3 encryption. In addition, BACnet/SC uses certificate management to help ensure only those devices authorized to be on a BACnet/SC network can operate on that network.

Native OPC UA Client support

OPC UA Client functionality is natively supported in Enterprise Server and field servers, enabling powerful and high-capacity integration of devices or systems that have OPC UA Server capability. OPC Unified Architecture (OPC UA) is a standard originating from industrial automation and process control that provides methods intended to provide improved security, performance, and engineering efficiency. With OPC UA Client support, the EcoStruxure Building Operation software can monitor and control a wide variety of devices or systems, from Schneider Electric as well as from other companies.

Native LonWorks support

The Enterprise Server works with a range of LonTalk adapters to communicate to TP/FT-10 LonWorks networks. Integrated LonWorks functionality enables access to LonWorks devices from Schneider Electric and other vendors. LonWorks networks can be commissioned, bound, and configured from the Enterprise Server using the built-in LonWorks Network Management Tool. No third-party tools are needed. To increase ease of use, LNS device plug-ins are supported. This allows for easier engineering and maintenance of LonWorks devices from Schneider Electric and other vendors. There are some limitations on how LNS device plug-ins can be used.

Native Modbus support

The Enterprise Server and field servers natively integrate Modbus RS-485 client and server configurations, as well as Modbus TCP client and server. This allows full access to third-party products and the range of Schneider Electric products that communicate on the Modbus protocol, such as power meters, UPS, circuit breakers, lighting controllers, and emergency lighting.

Modbus device types are pre-configured Modbus applications for quick and easy Modbus device integration in EcoStruxure Building Operation solutions.

Web Services support

The Enterprise Server supports the use of Web Services based on open standards, such as SOAP and REST, to consume data into the EcoStruxure BMS. Use incoming third-party data (temperature forecast, energy cost) over the Web to determine site modes, scheduling, and programming.

EcoStruxure Web Services support

EcoStruxure Web Services, Schneider Electric’s Web Services standard, is natively supported in the EcoStruxure BMS servers. EcoStruxure Web Services offers extra features between compliant systems whether within Schneider Electric or other authorized systems. These features include access to semantic model, system directory browsing, read/write of current values, alarm receipt and acknowledgement, and historical trend log data. EcoStruxure Web Services requires user name and password to log on to the system.

MQTT IoT protocol support

The Enterprise Server and field servers support MQTT as an option for publishing data to, and receiving updates from, other systems. MQTT is a messaging transport protocol that with its small footprint, light bandwidth utilization, and simplicity, is ideal for M2M and IoT communication. The MQTT capability supports communication with any MQTT broker, for example, Amazon, Microsoft, Google or IBM.

IT friendly

The EcoStruxure BMS servers communicate using the networking standards. This makes installations easy, management simple, and transactions more secure.

Supported Protocols
  • IP addressing

  • TCP communications

  • DHCP for easy network configuration

  • DNS for simple lookup of addresses

  • HTTP/HTTPS for internet access through firewalls, which enables remote monitoring and control

  • NTP (Network Time Protocol) for time synchronization throughout the system

  • SMTP or SMTPS with support for SSL/TLS based authentication, enables sending email messages triggered by schedule or alarm

  • SNMP enables reception of application alarms in designated network management tools

  • WebSocket Secure (WSS) and TLS 1.3 encryption (BACnet/SC applications)

TLS support

Communication between clients and the EcoStruxure BMS servers , and between EcoStruxure BMS servers, can be encrypted using Transport Layer Security (TLS ). The servers are delivered with a default self-signed certificate. Commercial Certification Authority (CA) server certificates are supported to lower the risk of malicious information technology attacks. Use of encrypted communication can be enforced for both WorkStation and WebStation access.

Table: Building Automation – Windows and Linux Licences Availablility

Enterprise Server Licenses

Windows

Linux

Enterprise Server - 10 automation servers a

Yes

Yes

Enterprise Server - 50 automation servers a

Yes

Yes

Enterprise Server - 100 automation servers a

Yes

Yes

Enterprise Server - 250 automation servers a

Yes

Yes

  1. For more information on the part numbers, see section “Specifications”, subsection “Part Numbers”.

Upgrade Software Bundle Licences

Windows

Linux

Upgrade 3.x - 10 automation servers a

Yes

-

Upgrade 3.x - 50 automation servers a

Yes

-

Upgrade 3.x - 100 automation servers a

Yes

-

Upgrade 3.x - 250 automation servers a

Yes

-

Upgrade 4.x or 5.x - 10 automation servers a

Yes

-

Upgrade 4.x or 5.x - 50 automation servers a

Yes

-

Upgrade 4.x or 5.x - 100 automation servers a

Yes

-

Upgrade 4.x or 5.x - 250 automation servers a

Yes

-

  1. For more information on the upgrade software bundles, see section “Specifications”, subsection “Upgrade software bundles”.

Add-on Option Licences

Windows

Linux

ES Hosting AS Pack - 01 a

Yes

Yes

ES Hosting AS Pack - 10 a

Yes

Yes

ES Hosting AS Pack - 50 a

Yes

Yes

ES Hosted Node Pack - 5 a

Yes

Yes

ES Hosted Node Pack - 10 a

Yes

Yes

ES Hosted Node Pack - 25 a

Yes

Yes

ES Hosted Node Pack - 50 a

Yes

Yes

ES Hosted Node Pack - 100 a

Yes

Yes

ES Hosted Node Pack - 300 a

Yes

Yes

ES Hosted Node Pack - 600 a

Yes

Yes

EcoStruxure Web Services Consume a

Yes

Yes

EcoStruxure Web Services Serve & Consume a

Yes

Yes

EcoStruxure Web Services Serve & Consume and Historical trend log data a

Yes

Yes

Web Services (Generic Consume) option a

Yes

Yes

Alarm notifications via SNMP option a

Yes

Yes

Smart Connector deployment license a

Yes

-

Personal Dashboards option a

Yes

Yes

TimescaleDB connection option a

Yes

Yes

Microsoft SQL Server connection option a

Yes

Yes

AVEVA PI System connection option a

Yes

Yes

Regulated Industries Compliance Pack option a

Yes

Yes

PDF signing option a

Yes

Yes

MQTT option a

Yes

Yes

Zoning option a

Yes

Yes

SAML Authentication option a

Yes

Yes

Semantic DB Plus 2 CPU Cores a

Yes

-

Semantic DB Plus 6 CPU Cores a

Yes

-

Semantic DB External Use Plus 2 CPU Cores a

Yes

-

Semantic DB External Use Plus 6 CPU Cores a

Yes

-

Sustainability Pack option a

Yes

Yes

OPC UA Client option a

Yes

Yes

  1. For more information on the add-on options, see section “Specifications”, subsection “Add-on options”.

Table: Fire Detection – Windows and Linux Licences Availablility

Enterprise Server Licenses

Windows

Linux

Enterprise Server 1 year on premise subscription duration a

Yes

-

Essential plan 1 year on premise subscription duration Enterprise Server a

Yes

-

Enhanced plan 1 year on premise subscription duration Enterprise Server a

Yes

-

Advanced plan 1 year on premise subscription duration Enterprise Server a

Yes

-

  1. For more information on the part numbers, see section “Specifications”, subsection “Part Numbers”.

Add-on Option Licences

Windows

Linux

Connected Device on premise 1 year 10-pack, EcoStruxure Building Operation a

Yes

-

  1. For more information on the add-on options, see section “Specifications”, subsection “Add-on options”.

Specifications

Hardware requirements
Processor power, memory, and storage capacity should be scaled upwards to accommodate targeted system size as impacted by the total quantity of automation servers and expected historical archiving. Enterprise Server is tested on many different servers with varying configurations. The typical configuration is an 8-core 3.6 GHz processor, 32 GB of memory, and SSD storage capacity of 1 TB.
Processor
Minimum: Intel Core i5 @ 2.0 GHz or equivalent
  
Recommended: Intel Core i5 @ 3.0 GHz or better
Memory
Minimum: 8 GB
  
Recommended: 16 GB or higher
Storage capacity
Minimum: 100 GB
  
Recommended: 1 TB
Storage device
Recommended: Enterprise Solid State Drive (SSD)
An Enterprise SSD is recommended to maintain the necessary speed and stability. The database and the binaries should both be installed on the Enterprise SSD.
Other devices
Microsoft mouse or compatible pointing device is required.
Software requirements
Operating systems – Enterprise Server for Windows
Microsoft Windows 10 (64-bit)
  
Microsoft Windows 11 a
  
Microsoft Windows Server 2012 R2 (64-bit)
  
Microsoft Windows Server 2016
  
Microsoft Windows Server 2019
  
Microsoft Windows Server 2022 a
The following Microsoft Windows 10 editions are supported: Pro and Enterprise.
The following Microsoft Windows 11 a editions are supported: Pro and Enterprise.
The following Microsoft Windows Server 2012 R2 editions are supported: Datacenter, Standard, Essentials, and Foundation.
The following Microsoft Windows Server 2016 editions are supported: Datacenter, Standard, and Essentials.
The following Microsoft Windows Server 2019 editions are supported: Datacenter, Standard, and Essentials.
The following Microsoft Windows Server 2022 a editions are supported: Datacenter, Standard, and Essentials.
Operating systems – Enterprise Server for Linux
OCI compliant container runtime on Linux x86-64
Quality assurance testing has been performed on, and support is provided with, Ubuntu 20.04 and 22.04 with Docker Engine version 20.10.00. Other deployment scenarios have not been tested by Schneider Electric. Product Support Services may require that potential issues can be reproduced in tested and supported environment for full support.
Required additional software – Enterprise Server for Windows
Microsoft .NET Framework 4.7.2 and later
The Microsoft .NET Framework is required by Software Administrator.
External log storage PostgreSQL option
Supported versions of PostgreSQL ( www.postgresql.org ) with matching version of TimescaleDB extension ( www.timescale.com ).
  
Note: To use compression for trend data, TimescaleDB 2.11 or later is required.
Quality assurance testing has been performed by Schneider Electric with TimescaleDB and PostgreSQL installed natively in Windows 10, Windows Server 2012, 2016, and 2019. Other deployment scenarios have not been tested by Schneider Electric.
External log storage Microsoft SQL option
Microsoft SQL Server versions under full support by Microsoft ( www.microsoft.com ).
The following Microsoft SQL Server editions are supported: Enterprise, Standard, and Express.
External log storage AVEVA PI System option
PI Web API 2021 SP3 and database compatible with that version
Quality assurance testing has been performed by Schneider Electric with PI Web API 2021 SP3, and database compatible with that version, installed on Windows Server 2019. Other deployment scenarios have not been tested by Schneider Electric.
Communication
TCP
Binary, port fixed, 4444
HTTP
Non-binary, port configurable, default 80
HTTPS
Encrypted supporting TLS 1.3, 1.2, 1.1 a , and 1.0 a , port configurable default 443
WSS a
Encrypted supporting TLS 1.3, port configurable
SMTP
Email sending, port configurable, default 25
SMTPS
Email sending, port configurable, default 587
SNMP
version 3
  
Application alarm distribution using trap
NTP
Time synchronization
BACnet
BACnet/IP, port configurable, default 47808
  
BACnet/SC, port configurable, no default port
  
BTL B-BC (BACnet Building Controller) a
  
BTL B-SCHUB (BACnet Secure Connect Hub) a
  
BTL B-OWS (BACnet Operator Workstation) a
OPC UA Client
Profile group UACore 1.03
Core Client Facet, Base Client Behaviour Facet a , AddressSpace Lookup Client Facet, Attribute Read Client Facet a , Attribute Write Client Facet a , DataChange Subscriber Client Facet a , Method Client Facet, UA-TCP UA-SC UA-Binary, SecurityPolicy – Basic256, SecurityPolicy – Basic256Sha256, User Token – Anonymous Facet, User Token – User Name Password Client Facet, DataAccess Client Facet, Base Event Processing Client Facet, and Historical Access Client Facet.
Modbus
Modbus TCP, client and server
  
Modbus RTU and ASCII, RS-485, client and server a
MQTT
MQTT over TLS, port configurable, default 8883
  
MQTT over TCP, port configurable, default 1883
  
MQTT over WebSocket Secure (WSS), port configurable, default 443
  
MQTT over WebSocket (WS), port configurable, default 80
Supports the following LonTalk adapters:
NIC709-PCI
  
NIC709-USB
  
NIC709-USB100
  
NIC709-IP
  
NIC852
Other protocols may be used for particular additional functionality. See Technical Documentation.
LNS
LNS version
OpenLNS
Installed on WorkStation PC
LonMark
Resource files version
14.00
Part numbers
Building Automation – Enterprise Server for Windows
Enterprise Server - 10, EcoStruxure Building Operation Enterprise Server license for a PC server, includes support for 10 automation servers , 3 concurrent clients , and 1 semantic database limited to 2 CPU cores
SXWSWESXX00010
Enterprise Server - 50, EcoStruxure Building Operation Enterprise Server license for a PC server, includes support for 50 automation servers , 3 concurrent clients , and 1 semantic database limited to 2 CPU cores
SXWSWESXX00050
Enterprise Server - 100, EcoStruxure Building Operation Enterprise Server license for a PC server, includes support for 100 automation servers , 3 concurrent clients , and 1 semantic database limited to 2 CPU cores
SXWSWESXX00100
Enterprise Server - 250, EcoStruxure Building Operation Enterprise Server license for a PC server, includes support for 250 automation servers , 3 concurrent clients , and 1 semantic database limited to 2 CPU cores
SXWSWESXX00250
Building Automation – Enterprise Server for Linux
Enterprise Server - 10, EcoStruxure Building Operation Enterprise Server for Linux license, includes support for 10 automation servers, and 3 concurrent clients
SXWSWESLX00010
Enterprise Server - 50, EcoStruxure Building Operation Enterprise Server for Linux license, includes support for 50 automation servers, and 3 concurrent clients
SXWSWESLX00050
Enterprise Server - 100, EcoStruxure Building Operation Enterprise Server for Linux license, includes support for 100 automation servers, and 3 concurrent clients
SXWSWESLX00100
Enterprise Server - 250, EcoStruxure Building Operation Enterprise Server for Linux license, includes support for 250 automation servers, and 3 concurrent clients
SXWSWESLX00250
Fire Detection – Enterprise Server for Windows
Enterprise Server 1 year on premise subscription duration
FFSEFOSES00012
Essential plan 1 year on premise subscription duration Enterprise Server
FFSEFOPES00112
Enhanced plan 1 year on premise subscription duration Enterprise Server
FFSEFOPEH00112
Advanced plan 1 year on premise subscription duration Enterprise Server
FFSEFOPAD00112
Upgrade software bundles
Building Automation – Enterprise Server for Windows
Enterprise Server Upgrade – 10 or fewer automation servers
Upgrades Enterprise Server, with 10 or fewer hosted automation servers, from EcoStruxure Building Operation software version 3.x to 6.0.
SXWSWESUP30010
Enterprise Server Upgrade – 50 or fewer automation servers
Upgrades Enterprise Server, with 50 or fewer hosted automation servers, from EcoStruxure Building Operation software version 3.x to 6.0.
SXWSWESUP30050
Enterprise Server Upgrade – 100 or fewer automation servers
Upgrades Enterprise Server, with 100 or fewer hosted automation servers, from EcoStruxure Building Operation software version 3.x to 6.0.
SXWSWESUP30100
Enterprise Server Upgrade – 250 or fewer automation servers
Upgrades Enterprise Server, with 250 or fewer hosted automation servers, from EcoStruxure Building Operation software version 3.x to 6.0.
SXWSWESUP30250
Enterprise Server Upgrade – 10 or fewer automation servers
Upgrades Enterprise Server, with 10 or fewer hosted automation servers, from EcoStruxure Building Operation software version 4.x or 5.x to 6.0.
SXWSWESUP40010
Enterprise Server Upgrade – 50 or fewer automation servers
Upgrades Enterprise Server, with 50 or fewer hosted automation servers, from EcoStruxure Building Operation software version 4.x or 5.x to 6.0.
SXWSWESUP40050
Enterprise Server Upgrade – 100 or fewer automation servers
Upgrades Enterprise Server, with 100 or fewer hosted automation servers, from EcoStruxure Building Operation software version 4.x or 5.x to 6.0.
SXWSWESUP40100
Enterprise Server Upgrade – 250 or fewer automation servers
Upgrades Enterprise Server, with 250 or fewer hosted automation servers, from EcoStruxure Building Operation software version 4.x or 5.x to 6.0.
SXWSWESUP40250
Add-on options
Building Automation – Enterprise Server for Windows
ES Hosting AS Pack - 01, License to add 1 automation server
in addition to the original Enterprise Server purchased size.
SXWSWASES00001
ES Hosting AS Pack - 10, License to add 10 automation servers
in addition to the original Enterprise Server purchased size.
SXWSWASES00010
ES Hosting AS Pack - 50, License to add 50 automation servers
in addition to the original Enterprise Server purchased size.
SXWSWASES00050
ES Hosted Node Pack - 5, License to add 5 Non-SpaceLogic servers/controllers.
SXWSWNDES00005
ES Hosted Node Pack - 10, License to add 10 Non-SpaceLogic servers/controllers.
SXWSWNDES00010
ES Hosted Node Pack - 25, License to add 25 Non-SpaceLogic servers/controllers.
SXWSWNDES00025
ES Hosted Node Pack - 50, License to add 50 Non-SpaceLogic servers/controllers.
SXWSWNDES00050
ES Hosted Node Pack - 100, License to add 100 Non-SpaceLogic servers/controllers.
SXWSWNDES00100
ES Hosted Node Pack - 300, License to add 300 Non-SpaceLogic servers/controllers.
SXWSWNDES00300
ES Hosted Node Pack - 600, License to add 600 Non-SpaceLogic servers/controllers.
SXWSWNDES00600
SW-EWS-1, EcoStruxure Web Services (run-time) option
Consume only for one Enterprise Server or one Enterprise Central
SXWSWEWSX00001
SW-EWS-2, EcoStruxure Web Services (run-time) option
Serve & Consume for one Enterprise Server or one Enterprise Central
SXWSWEWSX00002
SW-EWS-3, EcoStruxure Web Services (run-time) option
Serve & Consume, plus Historical trend log data for one Enterprise Server or one Enterprise Central
SXWSWEWSX00003
SW-GWS-1, Web Services (Generic Consume) option
For one Enterprise Server or one Enterprise Central
SXWSWGWSX00001
SW-SNMP-1, Alarm notifications via SNMP option
For one Enterprise Server or one Enterprise Central
SXWSWSNMP00001*
SW-SMART-CONNECT, Smart Connector deployment license
For one Smart Connector deployment
SXWSWSCDL100001
Building Operation Personal Dashboards option, 1 per server required for users logging on to that server to have Personal Dashboard capabilities
For one Enterprise Server or one Enterprise Central
SXWSWDASH00001
SW-ESDBTS-1, TimescaleDB connection option
For one Enterprise Server
SXWSWESDBTS001*
EcoStruxure Building Operation, Microsoft SQL Server connection option
For one Enterprise Server
SXWSWESDBMS001*
EcoStruxure Building Operation, AVEVA PI System connection option
For one Enterprise Server
SXWSWESDBPI001*
Regulated Industries Compliance Pack option
For one Enterprise Server or one Enterprise Central
SXWSWCMPLPK001*
SW-ESPDF-1, Building Operation PDF signing option
For one Enterprise Server
SXWSWESPDFSS01
SW-ESMQTT-1, MQTT option
For one Enterprise Server
SXWSWMQTTSRW01*
Building Operation Zoning option
For one Enterprise Server
SXWSWESSDZR001
SAML Authentication option
For one Enterprise Server
SXWSWESSAML001*
Semantic DB Plus 2 CPU Cores
Additional concurrent queries for one semantic database
SXWSWSTDBAC002
Semantic DB Plus 6 CPU Cores
Additional concurrent queries for one semantic database
SXWSWSTDBAC006
Semantic DB External Use Plus 2 CPU Cores
Enables queries from external tools and additional concurrent queries
SXWSWSTDBEUAC2
Semantic DB External Use Plus 6 CPU Cores
Enables queries from external tools and additional concurrent queries
SXWSWSTDBEUAC6
Sustainability Pack option
For one Enterprise Server for Windows
SXWSWESSUSPKW1*
OPC UA Client option
For one Enterprise Server for Windows
SXWSWESOPCLW01*
Building Automation – Enterprise Server for Linux
ES Linux Hosting AS Pack - 01, License to add 1 automation server
in addition to the original Enterprise Server for Linux purchased size.
SXWSWASESL0001
ES Linux Hosting AS Pack - 10, License to add 10 automation servers
in addition to the original Enterprise Server for Linux purchased size.
SXWSWASESL0010
ES Linux Hosting AS Pack - 50, License to add 50 automation servers
in addition to the original Enterprise Server for Linux purchased size.
SXWSWASESL0050
ES Linux Hosted Node Pack - 5, License to add 5 Non-SpaceLogic servers/controllers.
SXWSWNDESL0005
ES Linux Hosted Node Pack - 10, License to add 10 Non-SpaceLogic servers/controllers.
SXWSWNDESL0010
ES Linux Hosted Node Pack - 25, License to add 25 Non-SpaceLogic servers/controllers.
SXWSWNDESL0025
ES Linux Hosted Node Pack - 50, License to add 50 Non-SpaceLogic servers/controllers.
SXWSWNDESL0050
ES Linux Hosted Node Pack - 100, License to add 100 Non-SpaceLogic servers/controllers.
SXWSWNDESL0100
ES Linux Hosted Node Pack - 300, License to add 300 Non-SpaceLogic servers/controllers.
SXWSWNDESL0300
ES Linux Hosted Node Pack - 600, License to add 600 Non-SpaceLogic servers/controllers.
SXWSWNDESL0600
EcoStruxure Web Services (run-time) option
Consume only for one Enterprise Server for Linux or one Enterprise Central for Linux
SXWSWEWSL00001
EcoStruxure Web Services (run-time) option
Serve & Consume for one Enterprise Server for Linux or one Enterprise Central for Linux
SXWSWEWSL00002
EcoStruxure Web Services (run-time) option
Serve & Consume, plus Historical trend log data for one Enterprise Server for Linux or one Enterprise Central for Linux
SXWSWEWSL00003
Web Services (Generic Consume) option
For one Enterprise Server for Linux or one Enterprise Central for Linux
SXWSWGWSL00001
Alarm notifications via SNMP option
For one Enterprise Server for Linux or one Enterprise Central for Linux
SXWSWSNMPL0001
Personal Dashboards option, 1 per server required for users logging on to that server to have Personal Dashboard capabilities
For one Enterprise Server for Linux or one Enterprise Central for Linux
SXWSWDASHL0001
TimescaleDB connection option
For one Enterprise Server for Linux
SXWSWESDBTSL01*
Microsoft SQL Server connection option
For one Enterprise Server for Linux
SXWSWESDBMSL01*
AVEVA PI System connection option
For one Enterprise Server for Linux
SXWSWESDBPIL01*
Regulated Industries Compliance Pack option
For one Enterprise Server for Linux or one Enterprise Central for Linux
SXWSWCMPLPKL01*
PDF signing option
For one Enterprise Server for Linux
SXWSWESPDFSSL1
MQTT option
For one Enterprise Server for Linux
SXWSWMQTTSRWL1*
Zoning option
For one Enterprise Server for Linux
SXWSWESSDZRL01
SAML Authentication option
For one Enterprise Server for Linux
SXWSWESSAMLL01*
Sustainability Pack option
For one Enterprise Server for Linux
SXWSWESSUSPKL1*
OPC UA Client option
For one Enterprise Server for Linux
SXWSWESOPCLL01*
Fire Detection – Enterprise Server for Windows
Connected Device on premise 1 year 10-pack, EcoStruxure Building Operation
FFSEFOCDE00112