earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Device Administrator, FDP Server
Functionalities: Engineering
3/6/2025

Saving a List of Field Servers

You save a list of field servers in the Device Administrator so that you can restore the list.

Show More
action_close

You can add field servers as a list in Device Administrator.

After you create the list of field servers, you can save the list. The list includes only field servers that are connected through the IP network. The list does not include field servers that are connected through the USB device port.

When you open Device Administrator, it automatically displays the list that was displayed when you last closed Device Administrator.

To save a list of field servers
  1. In Device Administrator, on the Device Administrator Server List toolbar, click Save current server list .

  2. Select a location for the server list file.

  3. In the File name box, enter a file name.

  4. Click Save .

Note:

The list of field servers does not include field servers that are connected through the USB device port. The list includes only field servers that are connected through the IP network.

  • EcoStruxure BMS Server Administration Overview
  • Device Administrator Server List Toolbar
  • Device Administrator
  • Save a List of Field Servers
  • Opening a List of Field Servers
  • Connecting to an EcoStruxure BMS Server Using the IP Network