earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebStation
Functionalities: Trends
10/30/2025

Trend Chart Settings Dialog Box – Series Tab

Use the Series tab to change the settings and attach a calculation method to a trend chart series.

 
action_zoom_plus_stroke Series tab
Figure: Series tab

Table: Series Tab

Component

Description

Color 

Select a color for the series. For more information, see Changing the Color of a Trend Chart Series .

Series presentation  

Select a presentation type for the series. The series can be presented with a line, a discrete line, digital, or bars. For more information, see Trend Series .

Y-axis

Select to display the y-axis to the left or to the right.

Weight

Select the weight of the series.

Show markers

Select True to show a marker for each record. The marker can only be shown for lines and discrete lines, not for digital and bars.

Show events

Select True to show events.

Calculation method

Select the calculation method to calculate the recorded values before displaying the series in the trend chart. For more information, see Calculation Methods .

Delta over period

Select to apply a period to the delta calculation method. For more information, see Calculation Methods .

Period

Select the time span for which the calculation method is to be executed.

Custom period

When Custom period is selected, enter a custom time span for which the calculation method is to be executed.

Custom period alignment 

When Custom period alignment  is selected, enter the time when you want the custom period to start.

  • Trend Chart Series in WebStation
  • Trend Series
  • Changing the Color of a Trend Chart Series
  • Calculation Methods
  • Trend Chart Series Menu
  • Trend Chart Settings Dialog Box – X Axis Tab
  • Trend Chart Settings Dialog Box – Left Axis Tab