earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Builder View, Enterprise Central, Enterprise Server
Functionalities: Engineering, Import/Export
12/18/2025

Engineering Tools Overview

You engineer your system using the engineering tools.

Twisted Pair Adapter Engineering Tool Overview

Twisted Pair Adapter Engineering Tool is a standalone software that allows you to monitor, troubleshoot and upgrade firmware for all SpaceLogic™ Twisted Pair Adapter devices on a network, as well as generate reports. The tool can send troubleshooting requests to selected adapters such as triggering restart and blinking LEDs, while always showing a graphical overview of the network topology. With zooming and filtering, even monitoring large networks becomes manageable, supporting 64 connected devices.

Insight Sensor Engineering Tool Overview

Insight Sensor Engineering Tool is a free software for creating and testing masks, controlling what is detected by the SpaceLogic Insight-Sensor's People Count sensor.

Spreadsheet Overview

You use the Spreadsheet view to create and edit multiple objects and to save time.

For more information, see Spreadsheet Overview .

Bindings Overview

A binding is a connection between two or more variables for data exchange. In its simplest form, a binding consists of a source and a destination. The source supplies the value to the destination.

For more information, see Bindings Overview .

Text Reports Overview

A text report provides a simple and quick method of obtaining a customized view of object property attributes.

For more information, see Text Reports Overview .

Import and Export Overview

A solution or application is a user-created object or group of objects that perform a control process. Examples of creatable objects include networks, devices, programs, binding templates, graphics, trends, and alarms.

For more information, see Import and Export Overview .

Project Configuration Tool Overview

Project Configuration Tool, with Project Configuration Tool web client and WorkStation, is an offline engineering platform that is used for project configuration, virtual EcoStruxure BMS server configuration, and deployment. Project Configuration Tool supports the major communication protocols in the same way as other EcoStruxure Building Operation software products.

Vista Conversion Overview

To assess whether or not to convert a Vista system to an EcoStruxure BMS, you run an analysis of the Vista database export file to get information on the potential outcome of a conversion. The analysis is performed in TAC Vista Conversion Tool. If the analysis confirms that the Vista database is suitable for conversion, you can convert the database in TAC Vista Conversion Tool.

Continuum Conversion Overview

Conversion is the process by which a customer's site is moved from Andover Continuum's legacy Building Management System to the EcoStruxure BMS. The Continuum Conversion Tool takes an ASCII dump from the Continuum system and creates EcoStruxure Building Operation objects that correspond to the objects in the ASCII dump file.

HMI Kiosk Overview

HMI Kiosk allows you to configure AD v3 as a dedicated HMI for local access to EcoStruxure BMS servers.

  • EcoStruxure Building Management Overview
  • Spreadsheet Overview
  • Bindings Overview
  • Text Reports Overview
  • Import and Export Overview