earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Basic Functionality
5/4/2026

General Information Properties – Basic Tab

Use the Basic tab to configure and view the General Information properties.

 
action_zoom_plus_stroke General Information properties – basic tab
Figure: General Information properties – basic tab

Table: General Information Properties

Component

Description

Name

Displays the name of the object.

Description

Type a description that explains what the object is used for.

Note: When performing a fire detection system reload, the description is replaced with the description provided in the Fire Expert configuration.

Type

Displays the object type that defines the properties of the object.

Foreign address

Displays the address to a non-EcoStruxure Building Management product, for example a BACnet device.

Modified

Displays the date and time when the object was last modified.

Note 1

Type text that you display in a graphic or use when searching for the object.

Note 2

Type text that you display in a graphic or use when searching for the object.

Validation

Select the validation status of the object to keep track of which objects have passed or not passed the validation.

Executed by

Indicates the object is executed by a BACnet device. An empty field indicates the object is executed by a field server or Enterprise Server.

  • Object Properties