earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
5
How to

How to


Products: Commission, IP-IO , MP-C, MP-V, RP-C
Functionalities: Engineering, BACnet/IP devices
Product version: 3.0, 3.1, 3.2, 3.3
10/13/2021

Launching and Activating the eCommission SmartX Controllers Mobile Application

You launch and then activate the eCommission SmartX Controllers mobile application to create an account before you can perform any tasks.

Show More
action_close

Prior to using the eCommission SmartX Controllers mobile application at a job site, there are some preparations you must make to facilitate device commissioning.

For more information, see eCommission SmartX Controllers Mobile Application Overview .

Launching and Activating the eCommission Application

You launch and then activate the eCommission SmartX Controllers mobile application to create an account before you can perform any tasks.

For more information, see Launching and Activating the eCommission SmartX Controllers Mobile Application .

Downloading and Starting the eCommission Application

You download and start the eCommission SmartX Controllers mobile application to perform commissioning, flow balance, and checkout operations on BACnet/IP controllers.

For more information, see Downloading and Starting the eCommission SmartX Controllers Mobile Application .

Transferring an Application Image File to a Mobile Device

Image files are created by a WorkStation user and contain pre-engineered objects, properties, and values. Download an Image to a BACnet/IP controller to facilitate device commissioning tasks.

For more information, see Image Downloading .

To launch and activate the eCommission SmartX Controllers mobile application
  1. On the mobile device or Windows 10 laptop, open the eCommission application.

  2. In the Activation code box, type the code appropriate to the user role, using the exact spelling, capitalization, and spacing:

    User role

    Activation code

    Technician

    CommissioningTool

    Flow Balancer

    FlowBalance

    Installer

    Electrician

  3. Select ACTIVATE .

  4. If this is your first log in to the eCommission application, create an account:

    • In the Username box, type a username.

    • In the Password box, type a password. When selecting a password for the eCommission application, be sure it meets the following requirements:

      • Contains at least 8 characters in total

      • Contains at least 1 number

      • Contains at least 1 special character

      • Contains at least 1 upper-case character

      • Contains at least 1 lower-case character

      • Contains no more than 3 repeating identical characters

    • In the Confirm password box, type the password again.

Your eCommission application account is created. You can now use the application with your assigned role until the activation period expires.

  • Preparations
  • Downloading and Starting the eCommission SmartX Controllers Mobile Application